topleft
SKF Online Catalog

Online Catalog

SKF introduces unitized pinion seals for heavy duty applications

March 16, 2009

ELGIN, IL –SKF recently announced the availability of SKF Unitized pinion seals for heavy duty applications. The SKF Unitized pinion seal reduces temperature at the sealing lip, promotes error-free installation and extends service life.

The SKF Unitized pinion seal features a fluorelastomer sealing lip suited to handle high operating temperatures of the pinion application. Its patented Waveseal design sweeps oil back towards the bearing, allowing the seal to run cooler. The seal consists of a half metal ID, which allows heat to dissipate, and a half rubber ID, which maintains positive grip on the yoke surface and prevents leak path. The sealant across the Bore-Tite OD serves as a protective coating, also eliminating leak paths.

“The SKF Unitized pinion seal is an ideal choice for heavy duty applications that operate under extremely high temperatures,” said Leslie Kern, product development manager, heavy duty, SKF. “Its design features work together to dissipate heat, which in turn results in longer service life and greater product reliability.”

Additionally, the SKF unitized pinion seal contains an internal wear sleeve that provides an optional sealing interface and protects the yoke shaft.  The unitized design creates a one-piece installation, eliminating the need to stock or install wear sleeves. And an internal labyrinth design with multiple dirt lips prevents ingress of contamination. The SKF unitized pinion seal also features a thermoplastic bumper that ensures proper seal position during installation.

For more information about the new SKF unitized pinion seal, including interchanges and specifications, visit www.vsm.skf.com, or contact your local SKF representative.

Established in 1907, SKF is a leading global supplier of bearing and elastomeric products, solutions and related services, as well as linear motion and lubrication technologies. Headquartered in Gothenburg, Sweden, with technology centers in the Netherlands, Italy and the United States, SKF is a valued partner to original equipment manufacturers and a major supplier to the automotive, aerospace, heavy-duty/off-highway, marine and other industries.

#    #    #

March 16, 2009

For further information, please contact:

Katie Noga, Marketing Communications Manager, SKF, 800-323-8024 x4471, katie.l.noga@skf.com

Brian Salvatore, Harris, Baio & McCullough, 215-440-9800, brian@hbmadv.com


Search

US Flag